Shop Laptops at ToshibaDirect Get Support at Support.Toshiba.com
Effective January 1, 2008, the Department of Transportation through the Pipeline and Hazardous Materials Safety Administration will no longer allow loose lithium batteries in checked luggage.

Spare batteries are the batteries you carry separately from the devices they power. When batteries are installed in a device, they are not considered spare batteries.

You may not pack a spare lithium battery in your checked baggage.

You may pack spare lithium batteries in carry-on baggage.

Keep spare batteries in the original retail packaging, to prevent unintentional activation or short-circuiting.

If original packaging is not available, effectively insulate battery terminals by isolating spare batteries from contact with other batteries and metal. Place each battery in its own protective case, plastic bag, or package. Do not permit a loose battery to come in contact with metal objects, such as coins, keys, or jewelry.

For loose batteries, place tape across the battery's contacts to isolate terminals. Isolating terminals prevents short-circuiting.

There is generally no restriction on the number of spare batteries allowed in carry-on baggage. However, you may carry no more than two larger batteries, in the range of 100-300 watt hour rating. See examples below.

Professional woman on cellphone with brief case
Batteries
 
Although you may carry some devices and installed batteries in checked baggage, carrying them in carry-on baggage, when practical, is preferred. In checked baggage, ensure that devices remain switched off, either by built-in switch/trigger locks, by taping the activation switch in the “off” position, or by other appropriate measures.
Take steps to prevent crushing, puncturing, or putting a high degree of pressure on the battery, as this can cause an internal short-circuit, resulting in overheating.
 
3-Second Survey
How helpful was this article?
 Not very helpful  Somewhat helpful  very helpful
  While Toshiba has made every effort at the time of publication to ensure the accuracy of the information provided herein, such information is subject to change without notice. Toshiba provides no warranty with regard to this newsletter or any other information contained herein. All express or implied warranties, including the implied warranties of merchantability and fitness for a particular purpose and/or noninfringement of third party rights are hereby disclaimed. Toshiba assumes no liability for any damages incurred directly or indirectly from any technical or typographical errors or omissions contained herein. In no event shall Toshiba be liable for any incidental, consequential, special, or exemplary damages, whether based on tort, contract or otherwise, arising out of or in connection with this newsletter, or any information contained herein or the use thereof.

Copyright ©2008 Toshiba America Information Systems, Inc. All other trademarks are the property of their respective owners.
 
Connect with us on Facebook Connect with us on Twitter Connect with us on YouTube