Shop Laptops at ToshibaDirect Get Support at Support.Toshiba.com

Qosmio® — Your creativity unleashed

If it’s extreme performance you crave, our Qosmio® X500 Laptop Series is designed to satisfy. Wherever and whenever the mood hits, it delivers cutting-edge multi-core power and blazing-fast 3D graphics for high-end gaming, high-def entertainment or high-demand tasks. And it lets you create killer multimedia.

Intel® Core™ processors—
for pro-class performance.
Equipped with the Intel® Core™ i7 and i5 processors, the Qosmio® laptop delivers maximum processing power when you need it most. So you’ll fly through intense 3D games, creating and editing video, or enjoying music and photos. With Intel® Turbo Boost and Intel® Hyper-Threading Technology, you’ll get the performance you’d expect from pro-class components like this.
NVIDIA® GeForce
Audio that rocks the room.
Prepare to be spoiled. These PCs come with Dolby Home Theater®, truly transforming music, movies and gaming with more realistic dialogue and explosions, along with deeper bass and brighter treble tones. You’ll enjoy rich virtual surround sound—on headphones or through the booming harman/kardon® stereo laptop speakers. Or cheer to killer multi-channel surround sound through a home entertainment system. Either way, you’ll find yourself right in the middle of the performance.
LAPTOP Magazine's Best Notebooks Of The Year Award for Qosmio® X505-Q850
Dedicated graphics—for unprecedented fun.
When it comes to visuals, Qosmio® laptops will make you forget about limitations. NVIDIA® GeForce® GTS 360M GPUs provide premium dedicated graphics processing for the hottest FPS-intensive games, hyper-realistic 3D visuals delivered at lightning fast frame-rates, along with vibrant, lifelike scenes and dynamic character effects. They’re also ideal for watching HD flicks, seamless photo editing, creating more memorable home movies, and getting the most from Windows® 7.
The beauty of Blu-ray®
It’s time to enjoy the stunning audio and video you’ve been craving. With an integrated Blu-ray® disc player, the Qosmio® X500 laptop is your ticket to truly brilliant HD movies—on the go with a jaw-dropping 18.4” diagonal display, or splashed across a home theater with your laptop’s advanced A/V connections.

Select Qosmio® laptops feature:

LED Backlit Keyboard
With this cool-looking keyboard you’ll be able to keep on gaming even with the lights down. It’s great for playing on planes or in quiet corners of your favorite cafés.
LED Backlit Keyboard
Solid State Drive
Load chapters faster, and get to your files and other multimedia at nearly twice the speed of a traditional spinning drive.
learn more »
Solid State Drive
Toshiba Media Controller
Toshiba Media Controller lets you easily stream videos, music and pictures from the media library on your laptop across your entire home entertainment network.
learn more »

Our Top Selling Qosmio® Laptops

xhide feature

Solid State Drive (SSD)

Lightning fast while standing still, Solid State Drives.

Sometimes the best way to leap ahead is to simply stop moving. At least that’s true with the solid state drives now offered on select Toshiba laptops. Here’s how this great new technology works: Regular hard drives find data with a “head” that moves across a spinning disc. That takes precious milliseconds. But with solid state drives there are no moving parts. Your data is always poised and ready to burst forth at the blink of an eye. It’s just crazy quick.

Enter a new realm of reliability
Free of moving parts, your solid state drive is designed to last longer than a conventional spinning hard drive. And if you’re a seasoned traveler here’s more good news: it’s also four times as tough and uses up to 50% less power* in idle mode than the older technology. So if your laptop gets smacked while you’re slipping into the window seat, don’t worry. Your data has some of the most advanced protection available and you can work longer.

Relish the joys of big and fast
Solid state drives are almost two times* faster than conventional drives and big, too, holding up to 512GB. So you’ll be able to store and open your holiday photos like that, retrieve those monster spreadsheets or presentations in a flash, and launch even the largest software programs sooner than ever.

Say hi to high-speed gaming
When you’re fully embroiled in the drama, seconds seem like hours. But with your new Toshiba laptop you can load an entire game on one of our huge solid state drives, sit back and enjoy the fun. With no gaps in the action, and no pausing for new chapters, your days of waiting are over.

* 1.7~1.8x faster claim is based on comparison of PCMark05 HDD benchmark score between Toshiba notebooks equipped with SSD and HDD, respectively. Comparison of each test item may vary, and benchmark score for an SSD model on a certain single test item may be lower than its corresponding HDD model. Results were achieved on select models and configurations tested by Toshiba at the time of publication.

Connect with us on Facebook Connect with us on Twitter Connect with us on YouTube